¿Cómo podemos ayudarte hoy?

How can I access the runtime configuration on the Magelis XBTGT / HMIGTO using Vijeo Designer


There are two ways to access the runtime configuration depending on how it was configured in the Vijeo Designer project.

-2 Corner
-Top Left Corner

For the 2-corner option to work, you must touch the top left corner first, then the bottom right corner second in sequence. (Not at the same time). This action must be done within 1 second. You could also press the top right corner first, then the bottom left corner second.

For the Top-Left Corner option to work, you must wait until the actual application has started. Within 10 seconds, press the top left corner.