¿Cómo podemos ayudarte hoy?

What are the dimensions of the EMFP fuse pack assembly?

Issue
The dimensions of the fuse holders and their respective lead lengths are needed.

Product Line
EMFP

Environment
Meter Installation

Cause
There may be the need to ensure that the fuse holders will fit in a given space and whether the leads are long enough for the location of the meter and the source.

Resolution
The fuse pack is 2.5 inches long and 1 inch in diameter. The conductor is 18 inches long on both sides of the fuse pack.
See picture below of a single fuse holder:
EMFP