How is a non standard or unusual voltage level Low Voltage Transformer obtained from SquareD/Schneider Electric?
Issue:
Obtaining Low Voltage Transformer products from SquareD/Schneider Electric
Product Line:
LV Transformers
Environment:
Applies to Low Voltage (LV) Transformers by SquareD/Schneider Electric
Cause:
Applications may require a Low Voltage Transformer with characteristics such as non standard Voltage Levels, 50 Hz rating, K rating, Stainless Steel Enclosure, non standard Temperature Rise, etc, or combinations of such features
Resolution:
There are three ways to obtain Low Voltage Transformer products from SquareD/Schneider Electric:
1. Select common Transformer types out of the SquareD/Schneider Electric catalog or Digest
2. Authorized SquareD/Schneider Electric Distributors may generate a quotation using a software tool called Product Selectors on (EQM) Electronic Quote Management to configure LV Transformers with characteristics not found in the Digest
3. If an unusual Low Voltage Transformer cannot be found in the Digest or configured on the Product Selector, Authorized SquareD/Schneider Electric Distributors may be able to obtain a quotation for it from our Low Voltage Transformer Plant Quotations Group, with the assistance of their local SquareD/Schneider Electric Account Representative or Field Office.
Publicado para: Schneider Electric Mexico