¿Cómo podemos ayudarte hoy?

Do we have a submersible pump application for the controller inside card?

Issue:
Custom program application for the controller inside card for submersible pumps.

Product Line:
Altivar 61, Altivar 71

Environment:
All models and serial numbers

Cause:
None

Resolution:
At this present time there are no custom programs for the controller inside card specific for submersible pumps only.