¿Cómo podemos ayudarte hoy?

How much space is required to add a PM 800 Series Power Meter in a NQ Panelboard enclosure ?

Issue:
Space required to add a PM 800 Series Power Meter into a NQ Panelboard enclosure. Can this be Field installed ?

Product Line:
NQ Panelboards and Powerlogic Power Meters

Environment:
Metering distribution

Cause:
Field installation

Resolution:
The NQ Panelboard enclosure needs extra inches of mounting space, and Metering can tonly be Factory installed .
The Factory installed PM800 Series meter will occupy an enclosure that will be extended 7" in Width and 6" in Height from the Factory.

BCPM , or Branch Circuit Power Metering can be used in NQ Panels ,and be field installed for individual metering of branch breaker loads., See attached Bulletin

Schneider Electric Mexico

Documentos adjuntos
BCPM Installation Guide.pdf [1.18 MB]