What is the maximum starts for the ATS22 soft starters?
Issue:
The ATS22 capable of doing 20 starts per hour?
Product Line:
ATS22
ATS22
Environment:
All model numbers and serial numbers
All model numbers and serial numbers
Cause:
None
None
Resolution:
No, the ATS22 is not designed for 20 motor starts per hour. The standard maximum cycle must not exceed 4 to 6 starts per hour with the ATS22.
No, the ATS22 is not designed for 20 motor starts per hour. The standard maximum cycle must not exceed 4 to 6 starts per hour with the ATS22.
Publicado para: Schneider Electric Mexico