¿Cómo podemos ayudarte hoy?

PowerLogic PM5000 Series (PM5100, PM5300, PM5500) Installation and User Guide

Issue
PM5000 Series Installation and User Guide

Product Line
PM5110, PM5330, PM5340, PM5560, and PM5563

Environment
Installation, Datasheet, Configuration, Programming, Instruction bulletin, User Manual

Cause
Documentation is needed to configure and install a PM5000 series meter

Resolution
View attached User Guide and Installation Guide below for PM5100, PM5300, and PM5500 series meters.

Refer to Article FA234024 for Technical datasheet, Brochure, and Part number breakdown.

Refer to Article FA234017 for Register List. Note this can be also found under each new firmware folder released from the SE website (se.com).

The meter documentation is contained in this link in the documents tab: PM5000 Series Meter Documentation (Technical datasheets, Instruction sheets, and User guides). The guide that is used is dependent on the part number of PM5000 meter that is used.

Note:
If the inside FAQ link is not opening but global window popping up, please proceed as the following or copy it and open it a new window:
  • Click on the hyperlink like “FA234024”,
  • (1) The global window “Select Location for FAQ” appears,
  • (2) Select your location,
  • (3) Then select your Country,
  • then the hyperlink article will open.
Location request priory opening the hyperlinks articles attached.

Schneider Electric Mexico

Documentos adjuntos
PM5100_User_Guide.pdf.pdf [4.47 MB]
PM5100_Installation_Guide.pdf [5.36 MB]
PM5300_User_Guide.pdf [4.84 MB]
PowerLogic PM5RD Installation Guide.pdf [1.73 MB]
PM5300_Installation_Guide.pdf [5.81 MB]