¿Cómo podemos ayudarte hoy?

What is the flexible cable mechanism for the FAL and FHL circuit breaker?

Issue:
What is the flexible cable mechanism for the FAL and FHL circuit breaker?

Product Line:
9422 Circuit Breaker Disconnects, FAL and FHL breaker

Environment:
Products sold in the North America

Cause:
Need a flexible cable mechanism to operate a FA or FH unit mount circuit breaker

Resolution:

Part #Total LengthFlexible Lengthwith 9422A1 Handle
9422CFA30
36"
22"
9422CFA31
9422CFA50
60"
46"
9422CFA51
9422CFA10
120''
106''
9422CFA11


See instruction bulletin, 50006-370-01

For left-handed operation

Part #Total LengthFlexible Length
9422CFAL30
36"
22"
9422CFAL50
60"
46"
9422CFAL10
120''
106''


See instruction bulletin, 30072-450-72

See drawing, 9422_CFA_OUTLINE_001

Use 9422A handles

Note:

Cannot be used with FC, FI, FD, FG, and FJ breakers.

Schneider Electric Mexico

Explora más
Producto:
Rango:
Explora más
Producto:
Rango: