¿Cómo podemos ayudarte hoy?

Is there a lug able to accept (3) 600 kcmil wire/per phase, for a PTPJ36120G Busplug ?

Issue:
Lug available accepting (3) 600 kcmil wire per phase for a PTPJ36120G Busplug

Product Line:
I Line Busway

Environment:
Retrofitting Breaker lugs

Cause:
Wire Bending restrictions

Resolution:
AL1200P7KU Lug kit is able to accept (3) 600 kcmil wire and is not in violation of NEC wire bending restrictions, and can be used with P frame breaker busplug