¿Cómo podemos ayudarte hoy?

What is the default energy rollover value for ION meters?

Issue
A user would like to know the default rollover values of the various ION meters.

Product Line
ION meters

Environment
Energy Calculations

Cause
A user would like to know the default rollover values of the various ION meters.

Resolution
Below is a list of ION meters and their default rollover values:

NOTE: By default, some of the meters have a Default Rollover Value of 0. This disables the rollover feature. In this case the meter will continue to accumulate energy until it hits the Maximum Energy Value.
Meter NameDefault Rollover ValueMaximum Energy Value
ACM37100999,999,999
ACM37200999,999,999
ION620010,000,000999,999,999
ION63000999,999,999
ION730010,000,000999,999,999
ION733010,000,000999,999,999
ION735010,000,000999,999,999
ION7500999,999,999
ION755010,000,000999,999,999
ION7600999,999,999
ION765010,000,000999,999,999
ION77000999,999,999
ION83000999,999,999
ION84000999,999,999
ION85000999,999,999
ION860010,000,000999,999,999
ION865010,000,000999,999,999
ION88000999,999,999
PM800010,000,000999,999,999
ION900010,000,000999,999,999

To avoid losing any resolution of the energy accumulate value it is recommend that the roll-over be set to 10 000 000. 16777215 (=2^24-1) is the absolute limit imposed by the 32bit IEEE register format without loss of resolution on the stored number.

NOTE: For instructions on how to change the rollover values on ION meters, please refer to: FA209519

Schneider Electric Mexico

Explora más
Producto:
Rango:
Explora más
Producto: