Does the M221 have Class 1 Div 2 rating?
Is there documentation for the M221 meeting Class 1 Div 2 standards?
Product Line:
TM221 all processors and I/O modules.
Cause:
Documentation on the M221 meeting the Class 1 Div 2 standards.
Resolution:
Yes. The M221 product family is Class 1 Div 2 A, B, C, D rated. See attachment