¿Cómo podemos ayudarte hoy?

How many simultaneous MBP_MSTR insructions are supported on the Unity 65x CoPro port and NOE771x1

Issue:
Number of simultaneous MBP_MSTR insructions

Product Line:
Modicon Quantum CPU
Modicon Qunatum NOE

Resolution:
The Unity 65x PLC supports 4 simultaneous MBP_MSTRS's on the CoPro port and each NOE771x1 supports 16 simultaneous MB_MSTR's.