¿Cómo podemos ayudarte hoy?

Can I-Line busway be used for a single phase application?

Issue:
Single Phase use of 3 phase product

Product Line:
Busway

Environment:
I-Line II

Cause:
Application

Resolution:
Yes, 3Ø busway could be used and just two of the three phases connected to the 1Ø power source.
If a neutral is required then 4W busway is used to obtain the neutral.
The busway plug-in units, fusible or circuit breaker, would only require 1 or 2 of their 3 poles to be used.