¿Cómo podemos ayudarte hoy?

Do Speed-D Switchboards come with copper bus, neutral and ground?

Issue:
Speed-D switchboards that comes with copper bus, neutral and ground.

Product Line:
Switchboards

Environment:
Speed-D

Resolution:
The following Speed-D switchboards come standard with copper buss, neutral and ground:
SB324WS; SB344WS; SB346WS; SB348WS
SF346WS; SF348WS
The SF324WS and SF344WS Switchboards have Aluminum bussing, neutrals and grounds

Note attached drawing and look to the upper right at the " Catalog number Table"

Schneider Electric Mexico

Documentos adjuntos
SB324WS drawing.pdf [49.4 KB]