¿Cómo podemos ayudarte hoy?

Can the ATV71 with an encoder be used for positioning control?

Issue:
ATV71 positioning control using encoder.

Product Line:
ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, the ATV71 with an encoder is used for accurate speed control and not for control of position.
Contact the Automation group at (800) 468-5342 for systems to perform the positioning functions.