¿Cómo podemos ayudarte hoy?

How to program an input on the ATV12 to freewheel stop?

Issue:
Configure an ATV12 to freewheel stop

Product Line:
Altivar 12

Environment:
All serial numbers

Cause:
N/A

Resolution:
To program an input to freewheel stop on the ATV12 use the following steps from RDY:

Press enter to rEf
Turn clockwise to ConF press enter.
Turn clockwise to Full press enter.
Turn clockwise to Fun press enter.
Turn clockwise to Stt- press enter.
Turn clockwise to nSt press enter.
Select the input  to use for nSt press enter.
Esc back to the beginning and cycle power.