¿Cómo podemos ayudarte hoy?

Can the ATS48 run the motor faster than the line frequency?

Issue:
Control speed on ATS48

Product Line:
ATS48, Altistart 48

Environment:
All models and serial numbers

Cause:
None

Resolution:
The motor can only run as fast as the line frequency. The ATS48 is a soft starter and cannot vary the speed as a variable speed drive can.