¿Cómo podemos ayudarte hoy?

Video: What is the part number for the joint side plate cover?

Issue:
What is the part number for the joint side plate cover?

Product Line:
Busway

Environment:
I-Line II Busway

Cause:
Joint side plate cover replacement

Resolution:
The joint cover is called a Tie Channel and is part number 45216-108-01.The Tie channel part number 45216-108-01 is the universal tie channel covers for 800A thru 5000A I-Line II Indoor busway. Part number 45132-051-50 is a hardware bag assembly with 16 screws for fastening channels to joint sides, 8 screws are required for each side Tie Channel. See video below:

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: