¿Cómo podemos ayudarte hoy?

Where do I connect an external +24vdc power supply on the ATV630 process drive?

Issue:
External power supply connection

Product Line:
ATV630

Environment:
All models and serial numbers

Cause:
None

Resolution:
The external +24vdc power supply must be connected to terminals P24 and 0v.  The positive is P24 and the negative is 0v.
DO NOT connect the external power supply to +24v.
No programming changes are required.