¿Cómo podemos ayudarte hoy?

Video: Masterpact NW breaker installation into PZ4 Switchgear?

Issue:
Is there a video for Masterpact NW breaker installation into PZ4 Switchgear?

Product Line:
PZ4 Switchgear

Environment:
Maintenance

Cause:
Installation of Masterpact NW drawout breaker

Resolution:
The 3 Part Video Series covers the following:
  1. Introduces the cell and installing parts for the breaker installation
  2. Demonstrates breaker and chassis Clusters
  3. Demonstrates mechanically and remotely racking breaker in and out

Schneider Electric Mexico

Documentos adjuntos
Empty compartment kit for NW breakers 80298-022-04.pdf [84.24 KB]