¿Cómo podemos ayudarte hoy?

Is there a pre assembled cord set with flying leads to use with the BMXD**6402K module?

Issue:
Looking for a pre assembled cable for the 64 channel discrete X80 IO modules.

Product Line:
M340, X80, Telefast

Resolution:
Yes. There are pre assembled cord sets with flying leads available. Below are the part numbers:
BMXFCW303  (3m)
BMXFCW503  (5m)
BMXFCW1003  (10m)

***You will need a quantity of 2 for each module***