¿Cómo podemos ayudarte hoy?

What does the "Z" indicate on the end of the ATV61 and ATV71 part number?

Issue:
"Z" Suffix of the ATV61/71

Product Line:
ATV61 and ATV71 drives.

Environment:
ATV61H075M3Z....ATV61HD15M3Z, ATV61H075N4Z....ATV61HD75N4Z
ATV71H075M3Z....ATV71HD15M3Z, ATV71H075N4Z....ATV71HD75N4Z

Cause:
None

Resolution:
The "Z" indicates the drive does not come with the graphic display keypad terminal.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)