What is the height and width of the doors used with HCP and HCRU Nema 1 Panel boxes?
What are door's dimensions used with HCP and HCRU Nema 1 Panel boxes?
Product Line:
HCP /HCRU I line Panels
Environment:
Layout
Cause:
Location space restrictions
Resolution:
The Double doors for the 4 piece vented trims have different part number suffix's per the Box height. See below heights and associated suffix's
The attached drawing is for the base part number for the doors 80104-961
-01 = 50"
-02 = 59"
-03 = 68"
-04 = 86"