¿Cómo podemos ayudarte hoy?

Will a HOM2200BB branch breaker install into a SC816D200C Meter Main?

Issue:
Can a HOM2200BB branch breaker be install into a SC816D200C Meter Main?

Product Line:
Combination All in Ones and Meter Mains

Environment:
Application

Cause:
Clarification

Resolution:
No , the maximum Homeline branch breaker is100A and should be mounted in the bottom space of interior.