¿Cómo podemos ayudarte hoy?

How does the Realflo works when the Source in AGA-8 is set to Laboratory instead of Calculate?

When the source in AGA-8 is set to laboratory the user-entered values for relative density and heating value are used. When it's set to calculate the values are calculated by the flow computer.