¿Cómo podemos ayudarte hoy?

Cannot change from Local to Remote on my ATV312 drive, by holding the Mode button.

Issue:
ATV312 not changing from local to remote mode.

Product Line:
ATV312 series drives

Environment
Firmware version 5.1 IE56 and above.

Cause:
Recent firmware change.

Resolution:
As of firmware version 5.1 IE56, The ATV312 series drives can no longer be switched from local mode to remote.  In order to change the drive from local to remote, you perform a factory reset using the FCS parameter.