Should the HBLSDSA40 surge device be connected to a breaker?
Issue:
Installation question
Product Line:
Hubbel Surge Device
Environment:
Surge protection
Cause:
Installation and wiring
Resolution:
The Surge Protective Device (SPD) shall be installed on a dedicated 20-ampere, 2- or 3-pole circuit breaker, in accordance with NEC Article 285 and the our manufacturer's installation guidelines.
Publicado para: Schneider Electric Mexico