What are the part numbers for Altivar Process drives demo and motor cases?
Issue:
Altivar Process Demo and Motor cases part numbers.
Product Line:
ATV320, ATV340, ATV630 and ATV930
Environment:
All
Cause:
NA
Resolution:
Part number Description
DemoATV630 ATV630 demo on stand only.
DemoATV930 ATV930 demo on stand only.
DemoATV320 ATV320 demo on stand only.
DemoATV340 ATV340 demo on stand only.
DemoATVSIM Drive Simulator demo box with HMI, inputs, LED status and motor.
Units include individual hard-side carry cases, power cord,
cables for accessories (some demos), and user manual.
Ordering Information
The new demo displays can be purchased individually or as a group directly through Q2C. Orders typically take three to six weeks for delivery. Standard discount multipliers will apply.