¿Cómo podemos ayudarte hoy?

How to correct the system error code: 3008 in Scadapack ES?

Question:
How to correct the system error code: 3008 in Scadapack ES?

Answer:
The Status point in the 5000 series I/O is not being validated by the E-series configurator software.
The problem was the status point that was assigned is already been used ( see point address in points folder) causing the system error 3008.
To correct the problem, disable the Stat. Pt. (see details below) or assign a stat point number that was not used.

Schneider Electric Mexico

Documentos adjuntos
5000 Series IO Configuration.png [73.46 KB]