What is the InF8 Fault on the Altivar Process Drive?
Altivar Process Drive with InF8 Fault.
Product Line:
Altivar Process Drive
Environment:
All serial numbers for Altivar Process Drive
Cause:
Internal supply voltage out of range.
Resolution:
The internal power supplies of the control block are monitored, if one is out of range the INF8 fault occurs.
Remedies
- Check internal power supply (10V and 24V to COM)
- Check with SoMove which power supply is out of range.
- Depending on the result change control block