¿Cómo podemos ayudarte hoy?

Short cut Keys for Accutech Devices

  1. Press and hold the NEXT and ENTER buttons for one second, It will return to the main display.
  2. Press ENTER button for one second, The display will scroll and provide the following information like RF configurations, RF status, Hardware version, RF freq., Firmware version and if the network was attached or unattached.