Video: How to select a Low Voltage Transformer using the Product Selector
Issue:
Selecting the appropriate Low Voltage 1ph or 3ph Transformer for your specific application.
Product Line:
Three Phase LV Transformers - Energy Efficient - EX (DOE 2016)
Three Phase LV Transformers - Energy Efficient - EX, K-13 Rated (DOE 2016)
Single Phase LV Transformers - Energy Efficient - EE (DOE 2016)
Environment:
North American Products
Resolution:
The LV Transformer Selection Tool makes it easy to choose the correct product for your application. The following video shows how quickly you can determine which transformer meets your specifications:
Alternatively, follow steps 1-5 below to select a LV Transformer:
1) Select a the Product Type or sub set
2) Select the KVA rating
3) Select the primary voltage
4) Select the secondary voltage
5) Select any accessories required
Useful links:
Cross Reference Tool - find Schneider Electric equivalents for many obsolete and competitor products.
Documents and Download Center - access technical documents, CAD files, drawings, brochures and more.
Online Digest - access to the Digest LV Transformer pages
Additional Selection Criteria for LV Transformers
Minimum attributes required to select a transformer:
| |
| Three-phase (three wire to four wire) Single-phase (two wire or three wire) |
| Single Phase formula: Volts x Current = VA Three Phase formula: Volts x Current x v3 = VA Convert VA to kVA by dividing by 1000 |
| |
|