Is it possible to fit 42 EDB14020EPDBA breakers in a 400A Main Lug Only NF panel, 480/277V 3Ph 4W ?
How many EDB14020EPDBA breakers will mount into a 400A Main Lug Only NF panel, 480/277V 3Ph 4W ?
Product Line:
NF Panelboards
Environment:
Application
Cause:
Verification
Resolution:
The NF 84 circuit interior is actually two interiors bussed together. The bussing goes between ckts 41-43 and 42-44, so a two pole breaker cannot mount in those locations. Also, ckts 83 & 84 cannot accommodate a two pole breaker.