¿Cómo podemos ayudarte hoy?

Can multiple ground bars be installed in Schneider Electric panels?

Issue:
How many ground bars can be installed on Schneider/Square D panelboards?

Product Line:
NQ NF I-Line panels

Environment:
Products sold in North America

Resolution:
Multiple ground bars can be installed in panels, with no restrictions, other than the space to add them and making sure they do not hinder any wire bending spaces. All NEC codes must be followed which is the responsibility of the installer. Approval from the Local Authority having Jurisdiction may be required.