What are the product time lines of availability for NQO / NQOB / NQOD / NEHB/ NF panelboards
When were SQ D panelboards made and when did they become obsolete
Product Line:
NQO / NQOB / NQOD / NEHB/ NF panelboards
Environment:
History
Cause:
Reference
Resolution:
The NQO and NQOB Panels were developed for Lighting loads /Commercial /Industrial . 3 phase with plug on and Industrial Bolt On Q1/Q1B breaker interior features . NQO/NQOB was developed in late 1960’s till obsolescence in 1987.
The NQOD Panels were designed for bolt on and plug on QO/QOB breakers and was sold starting in 1987. It was obsoleted and replaced by the NQ panelboard in 2008.
The NEHB Panels were used for mainly 480Y/277V distribution, using EH/EHB Plug on and bolt on breakers. It was manufactured between 1983-1995.
The NF Series 0 Panelboard with ED EDB breakers was first introduced in 1995 to Oct. 2008 , afterwhich time the Series E1 started with the introduction of the NQ panelboards as well .
Publicado para: Schneider Electric Mexico