How do you wire an EMA SPD to a 30A 3 pole breaker?
Issue:
Is a wiring diagram available for the SSP EMA SPD?
Product Line:
SPD
Environment:
SSP EMA SPDs
Resolution:
Refer to the SurgeLogic EMA series Instruction Bulletin 8222-0014 for actual wiring diagrams. The EMA series terminals accept a range of 10 AWG to 2 AWG copper wire for the phase, neutral, and ground connectors.
Publicado para: Schneider Electric Mexico