Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What actuators are used with VS-8223-556,or (576), or (596) -5-12 valve assemblies?
Issue:
What actuators are used with the following assemblies
VS-8223-556-5-12
VS-8223-576-5-12
VS-8223-596-5-12

Product Line:
Valves and Actuator

Environment:
Maintenance

Cause:
Replacement Parts

Resolution:
VS-8223-556-5-12 = MS41-7153 (Proportional) / MF41-7153 (Floating) / AV-607-1 Linkage
VS-8223-576-5-12 = MS40-7173 (Proportional) / MF40-7173 (Floating) / AV-607-1 Linkage
VS-8223-596-5-12 = MS61-7203 (Proportional) / MF61-7203 (Floating) / Linkage NOT Req'd

**NOTE**
Proportional actuators are available as an assembly, but Floating actuators should
be purchased separately, with the valve and linkage kit.