¿Cómo podemos ayudarte hoy?

How to cross reference a VBS-9263 valve.

Issue:
What is the cross reference for the VBS-9263 valve with the same format as below;

VBS-9263-0-6-37
VBS-9263-0-6-38
VBS-9263-0-6-39
VBS-9263-0-6-03
VBS-9263-0-6-04

Product Line:
Valves and Actuator

Environment:
Maintenance

Cause:
Replacement

Resolution:

The (6) in the old part numbers indicated a special O-Ring that we used for the OEM Dri-Steem.
This was an OEM part and ever since we have improved our standard O-Ring with the (4) in the part number, Dri-Steem has stopped using the (6) version. They currently now use the standard (4) valves.
Whenever you see the (6) in the part number, just change it to (4).
Active parts listed would be:
VBS-9263-0-6-37 = VBS-9263-0-4-37
VBS-9263-0-6-38 = VBS-9263-0-4-38
VBS-9263-0-6-39 = VBS-9263-0-4-39
VBS-9263-0-6-03 = VBS-9263-0-4-03
VBS-9263-0-6-04 = VBS-9263-0-4-04