¿Cómo podemos ayudarte hoy?

What is the conductor size for the NQNL4 200% neutral?

Issue:
What is the conductor size allowed for the NQNL4 200% neutral?

Product Line:
Circuit breaker panelboards and accessories

Environment:
Installation

Cause:
Specification

Resolution:
The NQNL4 will accept up to (2) - 750 MCM or (4) - 1/0 to 300 MCM.