¿Cómo podemos ayudarte hoy?

How do you read run status on the ATV630 and ATV930 drives using profinet telegram 1?

Issue:
Read run status on ATV630 and ATV930 drives using profinet telegram 1.

Product Line:
Altivar ATV630 and ATV930 drive

Environment:
All

Cause:
Status word for run is bit 2

Resolution:

The second word in the input table on the profinet side is for status.
bit 2 is the enable or run operation.

Bit 2

Profi