¿Cómo podemos ayudarte hoy?

What are the replacements for VS8-9313-360-5-13, VS8-9313-360-4-10 and VS8-9313-360-5-12 Valve assemblies ?

Issue:
Do the VS8-9313-360-5-13, VS8-9313-360-4-10 and VS8-9313-360-5-12 have any replacements available

Product Line:
Valve and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
These were special OEM valve and actuators for TRANE. The actuators were the old obsolete MS-83013, with TRANE wiring harness. We no longer make these wiring harnesses.
The cross reference information is below:

VS8-9313-360-5-13 Will cross to the VB-9313-0-5-13 Valve Body + MP-371-600 Actuator + AV-395 Linkage Kit.  The customer can try to re-use the harness.
VS8-9313-360-4-10 Will Cross to the VB-7313-0-4-10 Valve Body + MP-371-600 Actuator + AV-391 Linkage Kit. The customer can try to re-use the harness.
VS8-9313-360-5-12 Will cross to the VB-9313-0-5-12 Valve Body + MP-371-600 Actuator + AV-395 Linkage Kit.  The customer can try to re-use the harness

Packing Kit for the Old valves still available and are:
VB-9313-0-4-10 =  YBA-635
VB-9313-0-5-12  =  YBA-652-2
VB-9313-0-5-13  =  YBA-652-2