¿Cómo podemos ayudarte hoy?

Is there an end tap box for I-Line bus parts CP502G10, CP504G10, CP506G10?

Issue:
End tap box for 225A to 600A part numbers CP502G10 ,CP504G10, CP506G10?

Product Line:
I Line Busway

Environment:
Products sold in North America

Resolution:
We offer End Cable Tap Boxes for the 225A thru 600A I-Line busway, see attached.
The part numbers to order would be  either CP502G12ETBB for bolt end or CP502G12ETBS for slot end mounting for the 225A Busway .
The same part number format is used to order the 400A and 600A End Tap boxes .The enclosure dimensions for the 225A unit are the same as the 400A and 600A units. See attached drawing for end tap box dimensions

Schneider Electric Mexico

Documentos adjuntos
CP502G10 and CP504G10 and CP506G10 End Cable Tap Box 225A-600A.pdf [54.26 KB]