Which replacement modules are suitable for the A, B, and C phases of the TVS4IMA24B21?
Which replacement modules are suitable for the A, B, and C phases of the TVS4IMA24B21?
Product Line:
Surgelogic
Environment:
EMA series Surge Protective Devices (SPDs)
Cause:
The surge protective device (SPD) is in an alarm state and needs repair parts.
Resolution:
The MA4IMA241 is the replacement module for each phase (A, B, and C) individually.