Is it possible to configure one port on the HMIGTU to communicate with a PLC on one subnet, and the other port to communicate to a PLC on a different subnet?
Can the HMIGTU communicate to devices on two different subnets?
Product Line:
HMIGTU
Resolution:
It is possible for an Magelis HMIGTU (HMIG3U or HMIG5U) to communicate to two PLC's on a different subnets.
I have attached a screen capture on how you would configure Vijeo Designer. The Runtime will automatically route the device to the Ethernet port on the correct subnet.