¿Cómo podemos ayudarte hoy?

Can a surge suppression device be added internally to any of our dry type transformers?

Issue:
Can the EX, EE or Epoxy Resin filled transformers be ordered with, or is their a field install kit that can be used to accept an internal SPD device?

Product Line:
Dry type Transformers

Environment:
Products sold in North America

Resolution:
No. Schneider does not offer internal surge protection to our transformers. However an external mounted SPD can be mounted either on the Primary or secondary side of the transformers. Please consult a local distributor for a separate mounted SPD  rated for the application.