¿Cómo podemos ayudarte hoy?

Is the VW3A1101 keypad compatible with the ATV320 Drive?

Issue:
VW3A1101 keypad compatibility with ATV320

Product Line:
Altivar 320

Environment:
All

Cause:
Compatibility

Resolution:
Yes, the ATV320 drive is fully compatible with the VW3A1101 keypad.
You can also utilize the OPEN / SAVE AS functions to upload / download from one ATV320 to another as long as the part numbers and firmware matches.