¿Cómo podemos ayudarte hoy?

Buck Boost: 208V input, 230V output, Single-phase, 60 load amp

Issue:
What low voltage buck boost transformer cal be used for  208V input, 230V output, Single-phase, 60 load amp

Product Line:
Low voltage transformers sold and supported in the USA.

Environment:
Application;selection

Resolution:
The closest we can get is from 208V to 229V, Part# 1.5S43F, need Qty 1, Wiring Diagram 4


URL => http://www.schneider-electric.us/support/index?page=content&country=US&lang=en&locale=en_US&id=FA110503