¿Cómo podemos ayudarte hoy?

Is there v3.51 Unity firmware for 140CPU53414x CPUs?

No. The v3.51 firmware was not released for the 140CPU53414x. Firmware version 3.50 will more than likely be the final release for the 534 Unity family of controllers.
The 140CPU53414B firmware is currently at v3.50. **if using the SFCCNTRL block do not use this version**

The 140CPU53414A Less than PV16 firmware is currently at v3.31.

Updated July 17th, 2019.

**Attached is each of these two firmware files.

Schneider Electric Mexico

Documentos adjuntos
140CPUX341X__PVLT16_V331.bin [800 KB]
140CPUX341X_SV350.bin [800 KB]