¿Cómo podemos ayudarte hoy?

Can the ground be replaced on a PQ3606G Busway Plug?

Issue:
What is the replacement ground unit in a PQ3606G busway plug?

Product Line:
I-Line Busway and accessories

Environment:
Maintenace

Cause:
N/A

Resolution:
Customer is looking for the replacement ground for a PQ3606G.  I found FA109182 which shows the following parts:

Only for Series 4 devices - see the nameplate to verify that you have a Series 4 device.
ground finger is 45201-554-01 (1 ea)
ground lug is 45118-056-50 (1 ea)
screw is 2142217161 (1 ea)
These parts will work with any 30, 60, 100 amp PQ Bus Plug (Ser 4).