¿Cómo podemos ayudarte hoy?

Can the MA41-7153-502 Smart X Actuator be adjusted to start at 10 DEG Travel

Issue:
What range of travel does the MA41-7153-502 actuator start at?

Product Line:
Valves and Actuators

Environment:
Application

Cause:
STAT Coordination

Resolution:
The Actuator's minimum travel setting starts at 30 DEG, so 10 DEG is not avialable . All 133 in. lbs. Force Smart X actuators, have this minimum travel setting